Support-Portal » REFERENCE_FEATURE_SYSTEM_NAME & REFERENCE_FEATURE_GROUP_ID (en)

Specifies the classification or feature group system used within the ARTICLE_FEATURES element. REFERENCE_FEATURE_SYSTEM_NAME contains the name of the classification system.
The associated ID to which the item is allocated within the classification system is saved in the field REFERENCE_FEATURE_GROUP_ID.

<REFERENCE_FEATURE_SYSTEM_NAME>ECLASS-5.1.4</REFERENCE_FEATURE_SYSTEM_NAME>
<REFERENCE_FEATURE_GROUP_ID>24-11-03-21</REFERENCE_FEATURE_GROUP_ID>

Requirements:

→ The element ARTICLE_FEATURES can occur several times per item
→ A classification system can be stated in every ARTICLE_FEATURES element
→ An item can be allocated to several classification systems
– For example ETIM, ECLASS-3.0, ECLASS-5.1.4, ECLASS-6.1, UNSPSC-7.0 and so on
→ It is also possible to add features and properties via FEATURE element to the classification system


⇦ back to overview of BMEcat elements