Support-Portal » DESCRIPTION_SHORT (en)

The item brief description or the item name is stated in the field DESCRIPTION_SHORT. This is a unique and explanatory designation of the offered product, which is also displayed in the search results.

<DESCRIPTION_SHORT>sample article 1</DESCRIPTION_SHORT>

Requirements:

Mandatory field
→ Minimum length: 10 characters
→ Maximum length: 80 characters
→ Please enter the precise item designation in the item name
→ Distinctive distinguishing features such as size, colour, width, material etc. should also be added
→ No HTML formatting is possible


⇦ back to overview of BMEcat elements