Support-Portal » SUPPLIER_AID (en)

The unique item number, which you use in your system as a supplier, is stated in the field SUPPLIER_AID. This is an alphanumeric mandatory field, under which a unique item number must be saved. Items without a SUPPLIER_AID are not processed by Mercateo Unite and are not shown in the shop.

<SUPPLIER_AID>XYZ000102</SUPPLIER_AID>

Requirements:

Mandatory field
→ Minimum length: 1 character
→ Maximum length: 29 characters
→ An item number can only be used in the catalogue once
→ Item numbers used twice are ignored, items are not displayed
→ Please do not use special characters such as commas, & and #
→ Please do not use any umlauts such as ö, ä, ü


⇦ back to overview of BMEcat elements