Support-Portal » Return conditions via CSV

Besides the standard return condition, up to three deviating return conditions can be defined for the items within a catalogue. After activation in the Mercateo system, you can control the allocation of your items to the corresponding returns conditions via a CSV file. The following steps are required for activation:

Inform Mercateo of return conditions

Please first contact your supplier manager at Mercateo. Your supplier manager will send you a supplier master data sheet (SDS) in the form of an Excel table. You must send this back completed. Please ensure that all information regarding returns conditions is correct and complete.
You will be informed by Mercateo as soon as all information is saved in the system. Following you can then transfer the allocation of the items to the corrsponding return conditions via CSV file. Data provision takes place via FTP.

Create CSV file

The CSV file consists of 2 columns and has the following structure:

SUPPLIER_AID;RETURN_CONDITION
123456;Option1
234567;Option2
9999;Option1
456789;Option3
A20-33;Option1
  • The item numbers must be unique and correspond to the item numbers in your catalogue.
  • Separator: Semicolon
  • The first row with the header SUPPLIER_AID;RETURN_CONDITION is mandatory information.
  • Items that fall under the standard return conditions are not included in the CSV file. The predefined standard is displayed for these items.

Transfer to Mercateo

After editing, save the Excel table for safety. Next, export the data as a CSV file:

File > Save as > File type: „CSV (separator-separated) (*.csv)“

Naming of the file:

catalogueID_returncondition.csv

Please note:

  • The catalogue-ID will be provided by Mercateo
  • Please keep the file naming. Without correct naming, the CSV file can either not be processed or not be assigned to the correct catalogue.

Transmission of the files:
The CSV file is transferred via FTP. The access data will be communicated to the supplier during onboarding. If you are an existing supplier, you already have the FTP login details.
Once you have created the CSV file, please contact support@unite.eu. Please indicate in the mail for which catalogue you would like to activate the file.
You then receive all further information from Mercateo.